Devkit MPC5744P rev.e data problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Devkit MPC5744P rev.e data problem

2,628件の閲覧回数
haoxue1027
Contributor V

Hello,

Now,I recevied the data which is changed from 0 to 2pi.

But I want  the value from -pi to pi.

So I set the program " if data > pi,  data = data-2*pi"

When the data <pi , the data is correct in the freemaster.

haoxue1027_1-1599533843752.pnghaoxue1027_1-1599533843752.png

But if the data >pi , the data is big negative numbers.

haoxue1027_0-1599533807942.pnghaoxue1027_0-1599533807942.png

Can you tell me why? how to change the data to [-pi pi]?

Any help will be appreciated.

best regards

hao

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,610件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @haoxue1027 ,

Have you tried to check the data type? Maybe the FreeMaster tries to display as integer and you stores in the MCU like float.

Hope this helps,

Marius

0 件の賞賛
返信

2,599件の閲覧回数
haoxue1027
Contributor V

@mariuslucianand hello,

I have found the reason.

Beacuse in the sincon block , the input theta is set to [-pi,pi].

But in my simulink, the input is 0 to 2pi.

Therefore, when the data is greater than pi, an abnormal data  is displayed.

best regards

hao