DSC_target_change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSC_target_change

Jump to solution
1,863 Views
hayaoki7
Contributor IV

hello

I want to retarget the MC56F83000-EVK motor application to his MC56F81666VLF.
Please tell me how to change it.
Or C:\MATLAB\R2022b\Add_Ons\Toolboxes\NXP_MBDToolbox_DSC\DSC_Platform_SDK\ for building with MC56F81666VLF
I have a folder called
I don't have MC56F81666VLF in DSC_Platform_SDK, do I have to make this? Please tell me how to create it if necessary.

thank you.
Best regards

0 Kudos
Reply
1 Solution
1,855 Views
SorinIBancila
NXP Employee
NXP Employee

Hello @hayaoki7,

You can go to the following link MCUXpresso SDK Builder to generate the SDK for your specific processor. I recommend to generate for the same version as the SDK in toolbox (2.7.3) in case there are some updates that are not supported by the toolbox.

Let me know if this helps you.

Best regards,

Bancila Sorin

View solution in original post

1 Reply
1,856 Views
SorinIBancila
NXP Employee
NXP Employee

Hello @hayaoki7,

You can go to the following link MCUXpresso SDK Builder to generate the SDK for your specific processor. I recommend to generate for the same version as the SDK in toolbox (2.7.3) in case there are some updates that are not supported by the toolbox.

Let me know if this helps you.

Best regards,

Bancila Sorin