More granular control of SPI timing on S32K1xx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

More granular control of SPI timing on S32K1xx?

ソリューションへジャンプ
1,444件の閲覧回数
ranulf
Contributor IV

Are there any functions that provide more granular control of SPI timing than is available in the MBDT S32K1xx SPI config block?

0 件の賞賛
返信
1 解決策
1,370件の閲覧回数
SorinIBancila
NXP Employee
NXP Employee

Hello,

The S32K1 toolbox is based on SDK. You can go and check the files included in 'S32_Platform_SDK/platform/drivers/src/lpspi'.

Also, can you provide more information about what SPI timing you want to control?

Best regards,

Bancila Sorin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,371件の閲覧回数
SorinIBancila
NXP Employee
NXP Employee

Hello,

The S32K1 toolbox is based on SDK. You can go and check the files included in 'S32_Platform_SDK/platform/drivers/src/lpspi'.

Also, can you provide more information about what SPI timing you want to control?

Best regards,

Bancila Sorin

0 件の賞賛
返信