Cannot program with RappID via CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot program with RappID via CAN

1,581 Views
AsierMaser
Contributor II

Hi everyone,

I have some trouble when I try to program my MPC5675K (custom board) via CAN. I am using RAppID BL Tool for that purpose (version 1.6.7.35) and as interface I tried with Vector's CANcaseXL and VN1630 with no luck.

In order to make things easier, I generated a basic program with some peripherals check (comms, IOs, ADCs, etc.). The .mot file was generated in Matlab with Motor Control Toolbox. Here is the configuration of RAppID.

AsierMaser_0-1687332549017.png

And this is the message I get when I try to program the micro.

AsierMaser_1-1687332675837.png

The ABS2, ABS0 and FAB pins are set by hardware as the message says. I also tried with different baud rates with no luck. Is there any detail am I missing?

Any help or ideas are welcome.

Best regards

0 Kudos
Reply
1 Reply

1,515 Views
AsierMaser
Contributor II

No one had this problem before?

0 Kudos
Reply