Can't recognize OpenSDA drive in Simulink but in Device Manager

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't recognize OpenSDA drive in Simulink but in Device Manager

225 Views
WWsmp
Contributor I

Hi,

 

I was trying to use MBDT on S32K144EVB. I was able to see OpenSDA port in Device Manager, file explorer as a USB thumb drive as D. But I Simulink couldn't recognize the drive.

weizhongsmp_0-1756474010674.png

If I use Custom with Drive D:, then Simulink would stuck in generating code after build. It doesn't seem to be able to download to the board. And the board seems to be in a loop as well trying to boot up, with red LED quickly flashes and green LED flashes 5 times.

 

I saw similar posts from other members and I couldn't fix the issue. I think it might have to do with this unrecognized OpenSDA drive.

 

Thanks,

 

0 Kudos
Reply
0 Replies