Can I use the step debug the project downloaded from MATLAB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use the step debug the project downloaded from MATLAB?

2,113件の閲覧回数
leo_wu
Contributor I

Hi NXP Team,

I have a question about debug, if I create a project through MBDtools, than download to the MCU. But some issue happened, and the issue can't be found by MATLAB simulink, is there have a debug tool like IDE's step debugger can use?  

if I use IAR as a compiler in MATLAB simulink, can I use IAR to do this?

Thanks.

0 件の賞賛
返信
2 返答(返信)

2,035件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

After the project is generated, you can import it into IAR IDE, but you'll have to do this manually (import the files, select the linker file provided by our toolbox [.icf file], same for the startup file, etc.). But there is another option for debugging - S32 Design Studio (for ARM / Power, depending on what platform you are using). For our latest toolboxes we provide a special file you can use with S32 Design Studio to import everything automatically - so if you are using S32K or MPC toolbox, we recommend you go on this path. 

Kind regards,

Razvan.

0 件の賞賛
返信

2,035件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

You can check this thread for details on how to import the code generated by our toolbox into S32 Design Studio IDE.

Kind regards,

Razvan.

0 件の賞賛
返信