Can I use the step debug the project downloaded from MATLAB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the step debug the project downloaded from MATLAB?

2,116 Views
leo_wu
Contributor I

Hi NXP Team,

I have a question about debug, if I create a project through MBDtools, than download to the MCU. But some issue happened, and the issue can't be found by MATLAB simulink, is there have a debug tool like IDE's step debugger can use?  

if I use IAR as a compiler in MATLAB simulink, can I use IAR to do this?

Thanks.

0 Kudos
Reply
2 Replies

2,038 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

After the project is generated, you can import it into IAR IDE, but you'll have to do this manually (import the files, select the linker file provided by our toolbox [.icf file], same for the startup file, etc.). But there is another option for debugging - S32 Design Studio (for ARM / Power, depending on what platform you are using). For our latest toolboxes we provide a special file you can use with S32 Design Studio to import everything automatically - so if you are using S32K or MPC toolbox, we recommend you go on this path. 

Kind regards,

Razvan.

0 Kudos
Reply

2,038 Views
constantinrazva
NXP Employee
NXP Employee

You can check this thread for details on how to import the code generated by our toolbox into S32 Design Studio IDE.

Kind regards,

Razvan.

0 Kudos
Reply