Can FD example for HVBMS S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can FD example for HVBMS S32K344

1,021件の閲覧回数
yassinechamam
Contributor III

Hi,

we are trying to connect the RD-K344BMU with RD33775ACNCEVB using the CAN FD. i am successfully debugging the hvbmu2_775a_read_s32ct on the board but as i understand from freemaster the TDEncoding is using TPL and not the CAN. How can i change the setup of the Model for it to use CAN and not TPL or is there a Project that is already made for CAN. 

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)