Can FD example for HVBMS S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can FD example for HVBMS S32K344

1,015 Views
yassinechamam
Contributor III

Hi,

we are trying to connect the RD-K344BMU with RD33775ACNCEVB using the CAN FD. i am successfully debugging the hvbmu2_775a_read_s32ct on the board but as i understand from freemaster the TDEncoding is using TPL and not the CAN. How can i change the setup of the Model for it to use CAN and not TPL or is there a Project that is already made for CAN. 

Labels (1)
Tags (3)
0 Kudos
Reply
0 Replies