CAN communication continuous output method of S32K144 MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN communication continuous output method of S32K144 MCU

556 次查看
autics
Contributor III

MBDT_CAN_Comm.png

I am using the S32K144 MCU board.

If the program is written on the board after the above Simulink configuration, the CAN signal output is good.
The problem is that the CAN signal is not output when the CAN line is physically disconnected and then reconnected as shown in the image below.
CAN output only by resetting or re-inputting power.

Is there any way to keep the signal coming out?

COnnector.png

 

0 项奖励
回复
0 回复数