CAN communication continuous output method of S32K144 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN communication continuous output method of S32K144 MCU

555 Views
autics
Contributor III

MBDT_CAN_Comm.png

I am using the S32K144 MCU board.

If the program is written on the board after the above Simulink configuration, the CAN signal output is good.
The problem is that the CAN signal is not output when the CAN line is physically disconnected and then reconnected as shown in the image below.
CAN output only by resetting or re-inputting power.

Is there any way to keep the signal coming out?

COnnector.png

 

0 Kudos
Reply
0 Replies