AMMCLIB COS_FLT wave fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AMMCLIB COS_FLT wave fault

ソリューションへジャンプ
254件の閲覧回数
Chris_Tigger
Contributor III

Hi, 

I've encountered a very strange problem. When using the Simulink model of the AMMCLIB library, the output of the floating-point cosine function has spikes. Why is this? I can use the sin function and the cos function in the Simulink standard library normally.I hope to get your help.

Chris_Tigger_0-1754322560482.png

matlab version : 2025a

AMMCLIB version: 1.1.22

Best Regards!
Chris Tigger
0 件の賞賛
返信
1 解決策
235件の閲覧回数
Chris_Tigger
Contributor III
The input can be -pi ~pi ,I think.
Best Regards!
Chris Tigger

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
236件の閲覧回数
Chris_Tigger
Contributor III
The input can be -pi ~pi ,I think.
Best Regards!
Chris Tigger
0 件の賞賛
返信