AMMCLIB COS_FLT wave fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMMCLIB COS_FLT wave fault

Jump to solution
1,634 Views
Chris_Tigger
Contributor III

Hi, 

I've encountered a very strange problem. When using the Simulink model of the AMMCLIB library, the output of the floating-point cosine function has spikes. Why is this? I can use the sin function and the cos function in the Simulink standard library normally.I hope to get your help.

Chris_Tigger_0-1754322560482.png

matlab version : 2025a

AMMCLIB version: 1.1.22

Best Regards!
Chris Tigger
0 Kudos
Reply
1 Solution
1,615 Views
Chris_Tigger
Contributor III
The input can be -pi ~pi ,I think.
Best Regards!
Chris Tigger

View solution in original post

0 Kudos
Reply
1 Reply
1,616 Views
Chris_Tigger
Contributor III
The input can be -pi ~pi ,I think.
Best Regards!
Chris Tigger
0 Kudos
Reply