AMMCLIB COS_FLT wave fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AMMCLIB COS_FLT wave fault

跳至解决方案
242 次查看
Chris_Tigger
Contributor III

Hi, 

I've encountered a very strange problem. When using the Simulink model of the AMMCLIB library, the output of the floating-point cosine function has spikes. Why is this? I can use the sin function and the cos function in the Simulink standard library normally.I hope to get your help.

Chris_Tigger_0-1754322560482.png

matlab version : 2025a

AMMCLIB version: 1.1.22

Best Regards!
Chris Tigger
0 项奖励
回复
1 解答
223 次查看
Chris_Tigger
Contributor III
The input can be -pi ~pi ,I think.
Best Regards!
Chris Tigger

在原帖中查看解决方案

0 项奖励
回复
1 回复
224 次查看
Chris_Tigger
Contributor III
The input can be -pi ~pi ,I think.
Best Regards!
Chris Tigger
0 项奖励
回复