ADC models’ simulation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC models’ simulation error

ソリューションへジャンプ
3,798件の閲覧回数
ca_liu
Contributor II

When I tested the ADC models,all of the four ADC models in S32K14x Exchange Projects have the same simulation error said:

Invalid setting in 'adc_software_trigger_s32k14x/ADC_Start' for parameter 'uint32(strcmp(out.aien, 'on'))'.
Caused by:
Expression 'uint32(strcmp(out.aien, 'on'))' for block 'adc_software_trigger_s32k14x/ADC_Start' returns an array of objects 

error.png

This is the first time that I have tested these ADC modules, and no changes have been made to them. I don't quite understand why this is happening and how I can solve it。

Can you give me some help?Thank you。

BTW,the version of MBDT is 2018.R1。

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,625件の閲覧回数
ca_liu
Contributor II

I reinstalled the mbdt, tested it, and there was no such error. So, it's possible that the installation problem caused the error.There is no more problem,thank you for your respond . Best wishes.

元の投稿で解決策を見る

4 返答(返信)
3,625件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Can you tell me if you have other (older) version of our toolbox installed? And on what version of MATLAB you are trying our models? Because I'm not able to reproduce your error. And one more question: when you say 'simulation error' do you mean an error that occurred on standard Simulink simulation (e.g.: clicking on the RUN button in Simulink) or on build (clicking on the Build Model button in Simulink)?

Best regards,

Razvan.

0 件の賞賛
返信
3,625件の閲覧回数
ca_liu
Contributor II

Hi Constantin Razvan Chivu,

I have installed other older version before,and have been updated directly to 2018.R1.Does that have anything to do with it?My Matlab version is 2018b.And the simulation error occurred in the standard Simulink simulation of clicking the RUN button.

I 'll try to uninstall the MDBT and reinstall it to see if I can solve the problem. I 'll get back to you when I have something.

Thank you.

0 件の賞賛
返信
3,626件の閲覧回数
ca_liu
Contributor II

I reinstalled the mbdt, tested it, and there was no such error. So, it's possible that the installation problem caused the error.There is no more problem,thank you for your respond . Best wishes.

3,625件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Thank you for pointing out that there are issues with our direct update - we'll investigate what happened; it seems to me that some files are not correctly updated.

Best regards,

Razvan.

0 件の賞賛
返信