ADC config in MBDT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC config in MBDT

600 次查看
paul_ephraim_13
Contributor III

I unable to edit the Adc Group Extra notification, as they seem to be disabled ! kindly help!
I am config for a S32k312- Q172 evb and in the interrupt block it displays pointing to nullptr.

i tried to replicate this model using an example provided in the nxp website
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Controlling-LED-intensity-with-ADC-and-PWM...

paul_ephraim_13_0-1726483511020.png

paul_ephraim_13_1-1726483728374.png

 

 



0 项奖励
回复
1 回复

571 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13,

First of all, I have some questions for you, namely, what is the reason for which you want to enable the Adc Group Extra Notification? What application do you want to implement so that you think you would need this feature? I ask to understand exactly what the use case is and the need to enable it, because this notification is implemented to be used simultaneously with the Adc_SetChannel API, a function that is currently not implemented in the ADC block.
It is possible that the functionality you want to implement does not necessarily require the use of this extra notification.

Keep us posted on your progress.

 

Best regards,

Dragos

 

0 项奖励
回复