ADC Hardware Averaging Question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC Hardware Averaging Question

3,042 次查看
sparkee
Contributor V

I need to know how the hardware averaging works so that I can use it effectively without altering my read timing.  I'm assuming that if I have a model that samples the ADC every 0.1ms using the PDB trigger and I set hardware averaging to 4 samples then I will get a sample every 0.4ms?  Or does the hardware averaging take my step size into account and sample every 0.025ms so that I get an averaged sample every 0.1ms?

For reference, I'm using a tapped delay to get an RMS value for the sine wave input signal and I need to know exactly how many delays I need.  I need to know if that RMS value goes above some threshold in a sample period.  For instance, if the RMS value goes above 100mV and stays for a period of 40ms, I want to trigger a flag.  If it crosses the threshold and dips back below in less than 40ms I will disregard it.  

pastedImage_1.png

标记 (1)
2 回复数

2,919 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello sparkee‌,

The best answer to the question "How does the ADC hardware averaging works" can be found in the Reference Manual from here https://www.nxp.com/webapp/Download?colCode=S32K1XXRM , the ADC chapter.

pastedImage_2.png

Now, all the toolbox does by enabling the HW ADC and samples to average checkboxes in the config block is to set the AVGE bit and the AVGS1 & AVGS0 bits. From what I've read, once you triggered a conversion, the hardware will perform as many conversions as selected [4, 8, 16, 32], and when it finishes the selected number, the averaging takes place. Once the average is computed, it will trigger the conversion complete interrupt. So, I don't think that the hw averaging takes the sample time into consideration at all. 

To be honest with you, I don't know how does that delay block works in generated code, if it is performing busy waiting or not.

Reading your explanations, reminded me of another hardware functionality: the Automatic compare function, which we also support in the configuration block. And what is nice about it is that the ADC can be set to provide the conversion result only if some threshold conditions are fulfilled. Please have a look at the following screenshots from the Reference Manual.

pastedImage_6.png

pastedImage_5.png

pastedImage_8.png

So I recommend you read the ADC functional description (Chapter 44.5 from the Reference Manual) and maybe my idea of taking into consideration the usage of the ADC automatic compare function may do your task easier. The only question remains how to measure those 40ms of above threshold time, but I think we can figure it out :smileygrin:.

Hope this helps,

Marius

2,919 次查看
sparkee
Contributor V

mariuslucianandrei to the rescue again, thank you.  I’ve read that section of the reference manual before but sadly did not make the right connection in my brain until you highlighted the lines.  I still had to read the line twice to make sure I understood it correctly.  I was mostly sure this was how the averaging worked but wanted to double-check so that I didn’t have major issues later.

 

As for the hardware compare, I was aware of this and planned to use it for one portion of my design but I'm needing to make multiple comparisons simultaneously so I'm trying to do that in software.  

Here's a shot of what I'm doing right now:

pastedImage_1.png

I'm nesting the delays so that I don't need a single tapped delay of 1000 delays.  I'm using hardware averaging at 4 then a 9 delay (plus current for 10 samples) then split out to more tapped delays to get 200/400/1000 samples for comparison.  I'll then compare those averages to my set points, which are different for each sample size.  The shorter the sample size, the higher the signal will have to be before I throw a flag.

Now that I'm walking through this I see there may be an issue with my logic on when to throw a flag so I'm going to have to think through this to make sure my approach will work for the desired outcome.

Thanks Marius!

0 项奖励
回复