while using Ethernet SDcard cannot be used

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

while using Ethernet SDcard cannot be used

2,098 Views
Swapnil_Enable
Contributor III

Hello,

i am working on a product using K60 controller + twr. i have used the RTCS and MFS library in development, as different module my code for MFS (data logging on SDcard) and Server/client codes are working fine.

when i downloaded only server/client code which is working fine. but when i insert the sdcard in the slot at the same moment the activity LED on Ethernet Socket goes OFF and connection is disconnected. and if i remove the Card from the slot the LED start glowing with resuming the connection.

now i am not able to understand why this is happening as when i checked the schematic of the tower board, i see no relation in the pins for sdcard and Ethernet.

Please help me i anyone now where to find the solution for the same.

Regards,

Swapnil

0 Kudos
Reply
3 Replies

1,768 Views
Swapnil_Enable
Contributor III

i found this link while searching on the topic.

https://community.freescale.com/thread/113946

https://community.freescale.com/message/116690

https://community.freescale.com/thread/302613

but i still don't understand what the solution.

0 Kudos
Reply

1,768 Views
c0170
Senior Contributor III

Hello,

I fixed your links in the previous post. Please, read link with number 116690 where is the explanation of Errata, and how to workaround this hw conflict.

If you have any further question, ask them there as they might assist you and discussion stays within same topic.

Regards,

MartinK

0 Kudos
Reply

1,768 Views
Swapnil_Enable
Contributor III

thanks kojto for fixing the links

0 Kudos
Reply