using lwevents in an ISR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

using lwevents in an ISR

跳至解决方案
2,323 次查看
Cdn_aye
Senior Contributor I

I need to debounce a switch on a GPIO port. I tried using waiting on a semaphore, having a task post (release) the semaphore after the debounce time but that doesn't seem to work in an ISR. Which I guess is reasonable because it seems that the task scheduler interacts with the semaphore calls and the ISR is not a task... or is this an error on my side.

I considered lwevents but I think they are plagued by the same problem. Is there 'best practice' someone could recommend for syncing the ISR to the debounced IRQ?

in the GPIO ISR

Interrupt

     process

     wait on semaphore or event

...

     resume

     clear interrupt flag

     return

Debounce Task

     delay

     post semaphore or event to ISR

     time wait (ticks)

Or should I just

ISR

diasable the interrupts

wait for the debounce task to run,

delay,

re-enable interrupts to ISR

I can probably get the last method to work but it is not very elegant.

Thanks

Robert

标记 (5)
0 项奖励
回复
1 解答
1,854 次查看
matthewkendall
Contributor V

You can't be waiting inside an ISR.

If you are going to have the pin trigger an interrupt then typical practice would be for the ISR to post an event to let the task know that the pin state has changed. In the task, block waiting for the event. When you get it, maybe wait for a short time then read the pin state. If it is still asserted, post an event to whatever other tasks need it.

If you have more than one input to scan (e.g. a keypad) then a more typical approach might be to just have the task scan all the keys say every 10ms. For each input have it maintain a record of the current physical state, the current logical state, and some counters. One of the counters would be the debounce counter; the logical state can change after the physical state has been constant for a short time. Other counters would handle short and long presses, auto-repeat, etc. The task can scan the inputs, post whatever events it has determined have happened, then sleep until the next scan.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,855 次查看
matthewkendall
Contributor V

You can't be waiting inside an ISR.

If you are going to have the pin trigger an interrupt then typical practice would be for the ISR to post an event to let the task know that the pin state has changed. In the task, block waiting for the event. When you get it, maybe wait for a short time then read the pin state. If it is still asserted, post an event to whatever other tasks need it.

If you have more than one input to scan (e.g. a keypad) then a more typical approach might be to just have the task scan all the keys say every 10ms. For each input have it maintain a record of the current physical state, the current logical state, and some counters. One of the counters would be the debounce counter; the logical state can change after the physical state has been constant for a short time. Other counters would handle short and long presses, auto-repeat, etc. The task can scan the inputs, post whatever events it has determined have happened, then sleep until the next scan.

0 项奖励
回复
1,854 次查看
Cdn_aye
Senior Contributor I

I could not get event flags or semaphores to work correctly from the ISR. What I was wondering was whether the reason they would work was there is nothing to pause in an ISR?? The debounce task could be paused but there was no event/semaphore mechanism to syc the isr and cause it to suspend until the debounce task was resumed. I agree any wait in an ISR could be a fatal mistake.


I got this to work by creating a debounce task. In the ISR disable interrupts, then enable the selection of the specific switch in the debounce task via a flag I set in the ISR. Then re-enable the IRQ's in the debounce task, and once the debounce was complete.

Thanks for the reply and advice

Regards

Robert

0 项奖励
回复