upload a file through the webserver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

upload a file through the webserver

ソリューションへジャンプ
1,805件の閲覧回数
Microfelix
Contributor IV

  

hello

I'm testing a card "TWR-K60" with CodeWarrior and I'd like to upload a file through the webserver. Is there an example? Maybe using the FTP-server? Can you explain how can I do?

 

thanks Maurizio

0 件の賞賛
返信
1 解決策
1,578件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

There are several example in the Freescale MQX3.7 release that have ftp capability.

Freescale MQX 3.7\mfs\examples\mfs_ftp

This is a good example.

You can FTP files to a USB stick connected to the TWRSER card.

Hope this helps.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,579件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

There are several example in the Freescale MQX3.7 release that have ftp capability.

Freescale MQX 3.7\mfs\examples\mfs_ftp

This is a good example.

You can FTP files to a USB stick connected to the TWRSER card.

Hope this helps.

Regards,

David

0 件の賞賛
返信