upload a file through the webserver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

upload a file through the webserver

Jump to solution
1,806 Views
Microfelix
Contributor IV

  

hello

I'm testing a card "TWR-K60" with CodeWarrior and I'd like to upload a file through the webserver. Is there an example? Maybe using the FTP-server? Can you explain how can I do?

 

thanks Maurizio

0 Kudos
Reply
1 Solution
1,579 Views
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

There are several example in the Freescale MQX3.7 release that have ftp capability.

Freescale MQX 3.7\mfs\examples\mfs_ftp

This is a good example.

You can FTP files to a USB stick connected to the TWRSER card.

Hope this helps.

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
1,580 Views
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

There are several example in the Freescale MQX3.7 release that have ftp capability.

Freescale MQX 3.7\mfs\examples\mfs_ftp

This is a good example.

You can FTP files to a USB stick connected to the TWRSER card.

Hope this helps.

Regards,

David

0 Kudos
Reply