udevd error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

udevd error

2,707件の閲覧回数
kecan
Contributor I

Imx6q core board, using 4.14.78 kernel, error reporting during startup. The error message is as follows:


INIT: version 2.88 booting
Starting udev
Udevd [206]: starting version 182
Imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
EXT4-fs (mmcblk3p3): mounting ext3 file system using the ext4 subsystem
EXT4-fs (mmcblk3p1): mounting ext3 file system using the ext4 subsystem
EXT4-fs (mmcblk3p3): mounted file system with ordered data mode. Opts: (null)
EXT4-fs (mmcblk3p1): mounted file system with ordered data mode. Opts: (null)
Udevd [206]: worker [209] timeout, kill it
Udevd [206]: SEQ 1546'/devices/soc0/soc/2100000.aips-bus/219c000.usdhc/mmc_host/mmc3/mmc3:0001/block/mmcblk3/mmcblk3 boot0 Killed'
Udevd [206]: worker [211] timeout, kill it
Udevd [206]: SEQ 1547'/devices/soc0/soc/2100000.aips-bus/219c000.usdhc/mmc_host/mmc3/mmc3:0001/block/mmcblk3/mmcblk3 boot1 Killed'
Udevd [206]: worker [220] timeout, kill it
Udevd [206]: SEQ 1551'/devices/soc0/soc/2100000.aips-bus/219c000.usdhc/mmc_host/mmc3/mmc3:0001/block/mmcblk3/mmcblk3rp'killed'
Random: crng init done

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,290件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the BSP that you are using is still in beta mode and is normal that could have these types of errors. Let me report it and see if there still a solution. However, I cannot guarantee anything because how I said, the BSP is still in beta mode and we cannot provide support of the beta's BSPs.

I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 件の賞賛
返信

2,290件の閲覧回数
kecan
Contributor I

Links we downloaded: repo init-u https://source.codeaurora.org/external/imx/imx-manifest-b imx-linux-sumo-m imx-4.14.78-1.0.0_ga.xml
Should this be an official release?

0 件の賞賛
返信

2,290件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize, I confirmed with the apps engineers and the BSP is officially released,  I can help you with the problem, I am checking for the solution. Just a question, are you using the demo image?

Best Regards,

Diego.

0 件の賞賛
返信