Problem with K60 TWR and Nand Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with K60 TWR and Nand Flash

1,763 Views
markdoxbeck
Contributor II

I have the K60 tower (TWRK60F120M), Code Warrior 10.6.4, and am using MQX 4.2.0.2. I am trying to run the nandflash_demo program but keep getting an error (when I run the demo).Here is the message I get:

 "Unable to open NAND flash device nandflash:"

This K60 Tower is supposed to have 2Gb of Nand Flash.

I have BSPCFG_ENABLE_NANDFLASH set to 1 (otherwise the demo would not compile).

What else do I need to do?

1 Reply

1,681 Views
markdoxbeck
Contributor II

I was able to utilize the Nand Flash by creating a new WORKSPACE.

For some unknown reason, my test workspace, which had over 20 different test programs in it, would not work with the Nand Flash.