udevd error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

udevd error

2,656 Views
kecan
Contributor I

Imx6q core board, using 4.14.78 kernel, error reporting during startup. The error message is as follows:


INIT: version 2.88 booting
Starting udev
Udevd [206]: starting version 182
Imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
EXT4-fs (mmcblk3p3): mounting ext3 file system using the ext4 subsystem
EXT4-fs (mmcblk3p1): mounting ext3 file system using the ext4 subsystem
EXT4-fs (mmcblk3p3): mounted file system with ordered data mode. Opts: (null)
EXT4-fs (mmcblk3p1): mounted file system with ordered data mode. Opts: (null)
Udevd [206]: worker [209] timeout, kill it
Udevd [206]: SEQ 1546'/devices/soc0/soc/2100000.aips-bus/219c000.usdhc/mmc_host/mmc3/mmc3:0001/block/mmcblk3/mmcblk3 boot0 Killed'
Udevd [206]: worker [211] timeout, kill it
Udevd [206]: SEQ 1547'/devices/soc0/soc/2100000.aips-bus/219c000.usdhc/mmc_host/mmc3/mmc3:0001/block/mmcblk3/mmcblk3 boot1 Killed'
Udevd [206]: worker [220] timeout, kill it
Udevd [206]: SEQ 1551'/devices/soc0/soc/2100000.aips-bus/219c000.usdhc/mmc_host/mmc3/mmc3:0001/block/mmcblk3/mmcblk3rp'killed'
Random: crng init done

Labels (1)
0 Kudos
Reply
3 Replies

2,239 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the BSP that you are using is still in beta mode and is normal that could have these types of errors. Let me report it and see if there still a solution. However, I cannot guarantee anything because how I said, the BSP is still in beta mode and we cannot provide support of the beta's BSPs.

I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos
Reply

2,239 Views
kecan
Contributor I

Links we downloaded: repo init-u https://source.codeaurora.org/external/imx/imx-manifest-b imx-linux-sumo-m imx-4.14.78-1.0.0_ga.xml
Should this be an official release?

0 Kudos
Reply

2,239 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize, I confirmed with the apps engineers and the BSP is officially released,  I can help you with the problem, I am checking for the solution. Just a question, are you using the demo image?

Best Regards,

Diego.

0 Kudos
Reply