timer example twrk60n512 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

timer example twrk60n512 problem

ソリューションへジャンプ
2,640件の閲覧回数
dingo
Contributor III

I have tried to run in IAR some projects in example folder of MQX but I have problem with "timer" project . The Make was unsuccessfully, the errors messages are attached. Also you have the whole "timer" project. Previously I have configured the user_config.h with  #define MQX_USE_TIMER 1 and have updated the bsp and psp projects.

 

Thank you for support

0 件の賞賛
返信
1 解決策
2,105件の閲覧回数
dingo
Contributor III

Hi David,

 

I  have found the problem, the PSP need to be "Rebuild All " but separate not with the whole build_libs.eww. Now the timer example work OK.

 

Thank you,

 

dingo

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,105件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Dingo,

I took your timer example and ran it using IAR6.10.5 and FSLMQX3.7 successfully on TWRK60N512.

Please ensure you are using IAR6.10.5 as IAR6.10.4 has compiler issues with FSLMQX3.7.

Hope this helps.

Regards,

David

PS

The release notes in the /doc folder let you know what version of tools work with current MQX version.

0 件の賞賛
返信
2,106件の閲覧回数
dingo
Contributor III

Hi David,

 

I  have found the problem, the PSP need to be "Rebuild All " but separate not with the whole build_libs.eww. Now the timer example work OK.

 

Thank you,

 

dingo

 

0 件の賞賛
返信