- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I want to deactivate kernel logging because I don't need it, to decrease the size of MQX in my application and to reduce CPU use by MQX. The problem is that when I disable this option ("#define MQX_KERNEL_LOGGING 0" in mqx_cnfg.h file), the PSP doesn't compile anymore. I get the following problem:
-> Undefined identifier 'kernel_data' in lwevent.c
In file mqx_prv.h, macros _KLOG and _KLOGM are defined as follow if MQX_KERNEL_LOGGING is set to 0:
#define _KLOGM(x)
#define _KLOG(x)
The problem is that when kernel_data is defined as in file lwevent.c ( _KLOGM(KERNEL_DATA_STRUCT_PTR kernel_data); ), preprocessor will remove this statement and compiler will say that kernel_data is undefined. I solved this problem by modifying the previous lines as follow:
#define _KLOGM(x) x
#define _KLOG(x)
Does anyone see a counter indication to this modification?
Thanks
Hugo
Solved! Go to Solution.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Daniel,
Thanks for the answer. I haven't tested with CodeWarrior 10.6 because it might compile properly without giving me the compiler error but I wouldn't be able to have the menu File->New->MQX 4.1 Project anymore which is only compatible with 10.5.
I can't migrate to 4.2 as we are using a Power PC microcontroller. Power PC are no more supported in MQX 4.2
Regards,
Hugo


- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Hugo:
I think this issue maybe related to the compile tools. Which IDE and the exact version you are using?
Regards
Daniel

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Daniel,
We are using CW 10.5 Build Id:130916 with the compiler provided with it.
Regards,
Hugo


- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
HI Hugo:
According to MQX 4.1 release notes, the development tools requirements is Codewarrior 10.6. I tested this case with MQX4.1.1 + CW10.6 +FRDMk64, #define MQX_KERNEL_LOGGING 0" in mqx_cnfg.h, not found this issue.
Regards
Daniel

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Daniel,
Thanks for the answer. I haven't tested with CodeWarrior 10.6 because it might compile properly without giving me the compiler error but I wouldn't be able to have the menu File->New->MQX 4.1 Project anymore which is only compatible with 10.5.
I can't migrate to 4.2 as we are using a Power PC microcontroller. Power PC are no more supported in MQX 4.2
Regards,
Hugo