linker file problems in KDS MQX 4.2 example project, for twrk60f120m

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linker file problems in KDS MQX 4.2 example project, for twrk60f120m

Jump to solution
1,976 Views
cavebiker
Contributor V

Hello,

I need to modify the linker file. I am trying to modify an example project in MQX 4.2 using KDS to run with KBOOT (uTasker serial loader)

I found intflash.ld, modified it, but when I build the project, KDS created a new intflash.ld file that is the same as the original.

Thanks in advance,

Tom

Tags (1)
0 Kudos
Reply
1 Solution
1,746 Views
cavebiker
Contributor V

I got it, I was modifying the wrong linker file. The file I needed to modify is in a different directory: > \Freescale_MQX_4_2\mqx\source\bsp\BSP_K60f12_to_K20FX_M12\gcc_arm\intflash.ld

Cheers!

View solution in original post

0 Kudos
Reply
2 Replies
1,747 Views
cavebiker
Contributor V

I got it, I was modifying the wrong linker file. The file I needed to modify is in a different directory: > \Freescale_MQX_4_2\mqx\source\bsp\BSP_K60f12_to_K20FX_M12\gcc_arm\intflash.ld

Cheers!

0 Kudos
Reply
1,746 Views
soledad
NXP Employee
NXP Employee

Hello Tom,

Thank you for your input :smileywink:

Regards

Sol

0 Kudos
Reply