linker file problems in KDS MQX 4.2 example project, for twrk60f120m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linker file problems in KDS MQX 4.2 example project, for twrk60f120m

ソリューションへジャンプ
1,982件の閲覧回数
cavebiker
Contributor V

Hello,

I need to modify the linker file. I am trying to modify an example project in MQX 4.2 using KDS to run with KBOOT (uTasker serial loader)

I found intflash.ld, modified it, but when I build the project, KDS created a new intflash.ld file that is the same as the original.

Thanks in advance,

Tom

タグ(1)
0 件の賞賛
返信
1 解決策
1,752件の閲覧回数
cavebiker
Contributor V

I got it, I was modifying the wrong linker file. The file I needed to modify is in a different directory: > \Freescale_MQX_4_2\mqx\source\bsp\BSP_K60f12_to_K20FX_M12\gcc_arm\intflash.ld

Cheers!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,753件の閲覧回数
cavebiker
Contributor V

I got it, I was modifying the wrong linker file. The file I needed to modify is in a different directory: > \Freescale_MQX_4_2\mqx\source\bsp\BSP_K60f12_to_K20FX_M12\gcc_arm\intflash.ld

Cheers!

0 件の賞賛
返信
1,752件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Tom,

Thank you for your input :smileywink:

Regards

Sol

0 件の賞賛
返信