install MQX 4.2 in KDS 3 on linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

install MQX 4.2 in KDS 3 on linux

跳至解决方案
1,473 次查看
garabito
Contributor III

Hi Everybody:

i download a KDS 3.0.0 and MQX 4.2 but i don't know how i can install the MQX 4.2 cause this is in source code, and not a installer.

Thanks

Carlos Enrique

1 解答
1,068 次查看
soledad
NXP Employee
NXP Employee

Hello Carlos,

In addition you can check the below thread,

Creating a New MQX RTOS 4.2 project in KDS


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,068 次查看
garabito
Contributor III

Sorry, i found how to do it in the next link

How To: Get Started with MQX RTOS for Kinetis SDK v1.1

thanks any way

Carlos Enrique

0 项奖励
回复
1,069 次查看
soledad
NXP Employee
NXP Employee

Hello Carlos,

In addition you can check the below thread,

Creating a New MQX RTOS 4.2 project in KDS


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------