install MQX 4.2 in KDS 3 on linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

install MQX 4.2 in KDS 3 on linux

Jump to solution
1,541 Views
garabito
Contributor III

Hi Everybody:

i download a KDS 3.0.0 and MQX 4.2 but i don't know how i can install the MQX 4.2 cause this is in source code, and not a installer.

Thanks

Carlos Enrique

1 Solution
1,136 Views
soledad
NXP Employee
NXP Employee

Hello Carlos,

In addition you can check the below thread,

Creating a New MQX RTOS 4.2 project in KDS


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,136 Views
garabito
Contributor III

Sorry, i found how to do it in the next link

How To: Get Started with MQX RTOS for Kinetis SDK v1.1

thanks any way

Carlos Enrique

0 Kudos
Reply
1,137 Views
soledad
NXP Employee
NXP Employee

Hello Carlos,

In addition you can check the below thread,

Creating a New MQX RTOS 4.2 project in KDS


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------