httpsrv example on FRDM-K64F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

httpsrv example on FRDM-K64F

跳至解决方案
5,267 次查看
mittymcdoogle
Contributor III

Hi,

I've tried running the httpsrv example code found in the MQX 4.2 package on my K64 freedom board. However, when I try to use the command prompt to ping the board, I fail to receive any response.

What can I do to get this demo working on my board?

Thanks,

Mitty

标记 (3)
0 项奖励
回复
1 解答
4,866 次查看
DavidS
NXP Employee
NXP Employee

Hi Mitty,

Try the following to cause your frdm-k64f Freedom board to do a DHCP:

Starting HTTP server No.0 on IP 192.168.1.202, port 80...[OK]

Shell (build: Jul  6 2015)

Copyright (c) 2013 Freescale Semiconductor;

shell>

shell> ipconfig dhcp

Bind via dhcp successful.

shell>

shell> ipconfig

Eth#     : 0

Link     : on

MTU      : 1500

MAC      : 00:00:5e:a8:01:ca

IP4      : 10.0.1.187 Type: DHCPNOAUTO

IP4 Mask : 255.255.255.0

IP4 Gate : 10.0.1.1

IP4 DNS  : 10.0.1.1

IP6      : DISABLED

Link status task stopped

shell>

shell> ping 10.0.1.1

Pinging 10.0.1.1:

Press [q] to cancel.

Reply from [10.0.1.1]: time=8ms

Reply from [10.0.1.1]: time=3ms

Reply from [10.0.1.1]: time=4ms

Reply from [10.0.1.1]: time=4ms

shell>

Regards,

David

在原帖中查看解决方案

9 回复数
4,866 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Mitty:

I think you can check the jumper settings in your board. Please refer to section 9.3 FRDM-K64F in MQX_Getting_Started.pdf.


Have a nice day,
Daniel

0 项奖励
回复
4,866 次查看
mittymcdoogle
Contributor III

Hi Daniel,

I don't see any jumper settings for Ethernet - were you just asking that I check my jumpers versus the default jumper configuration?

Thanks,

Mitty

0 项奖励
回复
4,866 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Mitty

Yes, the default jumper configurations is OK

I can run this demo in FRDM-K64 without problems.   please see the following picture, 192.168.1.10 is my PC's IP

pastedImage_0.png

0 项奖励
回复
4,866 次查看
mittymcdoogle
Contributor III

Hi Daniel,

I have checked all of my jumpers to make sure that they are set to the default position. I am still unable to ping the board or see the board through my router.

0 项奖励
回复
4,867 次查看
DavidS
NXP Employee
NXP Employee

Hi Mitty,

Try the following to cause your frdm-k64f Freedom board to do a DHCP:

Starting HTTP server No.0 on IP 192.168.1.202, port 80...[OK]

Shell (build: Jul  6 2015)

Copyright (c) 2013 Freescale Semiconductor;

shell>

shell> ipconfig dhcp

Bind via dhcp successful.

shell>

shell> ipconfig

Eth#     : 0

Link     : on

MTU      : 1500

MAC      : 00:00:5e:a8:01:ca

IP4      : 10.0.1.187 Type: DHCPNOAUTO

IP4 Mask : 255.255.255.0

IP4 Gate : 10.0.1.1

IP4 DNS  : 10.0.1.1

IP6      : DISABLED

Link status task stopped

shell>

shell> ping 10.0.1.1

Pinging 10.0.1.1:

Press [q] to cancel.

Reply from [10.0.1.1]: time=8ms

Reply from [10.0.1.1]: time=3ms

Reply from [10.0.1.1]: time=4ms

Reply from [10.0.1.1]: time=4ms

shell>

Regards,

David

4,866 次查看
mittymcdoogle
Contributor III

I plugged a new board into my router and I'm able to connect after using that command.

Thanks!

4,866 次查看
DavidS
NXP Employee
NXP Employee

WowWho!!!

Thanks for update.

Regards,

David

0 项奖励
回复
4,866 次查看
mittymcdoogle
Contributor III

Hi David,

When I type "ipconfig dhcp", I receive the following error message:

Error during dhcp bind 00001d04!

Thanks,

Mitty

0 项奖励
回复
4,866 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Mitty:

Check that the devices are in the same local subnet. Or, if they are in different subnet, make sure the gateway configuration in RTCS is correct. When RTCS tries to send an IP to different network, it sends the frame via gateway.

If it does not help, could you change another board and try it again?

Daniel

0 项奖励
回复