how I can measure execution time of u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how I can measure execution time of u-boot

3,315 Views
abdulraoof_numa
Contributor I

Hello Mr. Yuri

I got the source code of u.boot for imx6ultalite evaluation kit ,my question is how I can measure execution time of u-boot source code in eclipse IDE ….and uboot source code have many folders ..where I have to edit in order to have execution time ?

Thanks

Reagrds

Abdul

0 Kudos
Reply
1 Reply

3,090 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the following may help

[U-Boot] u-boot - timestamp 

CONFIG_TIMESTAMP should be defined:

#define        CONFIG_TIMESTAMP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply