how I can measure execution time of u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how I can measure execution time of u-boot

3,369件の閲覧回数
abdulraoof_numa
Contributor I

Hello Mr. Yuri

I got the source code of u.boot for imx6ultalite evaluation kit ,my question is how I can measure execution time of u-boot source code in eclipse IDE ….and uboot source code have many folders ..where I have to edit in order to have execution time ?

Thanks

Reagrds

Abdul

0 件の賞賛
返信
1 返信

3,144件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the following may help

[U-Boot] u-boot - timestamp 

CONFIG_TIMESTAMP should be defined:

#define        CONFIG_TIMESTAMP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信