getServiceByContractID return an error 0x80040154 when run/debug TWRK40X256QSDLAB MQX3.7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

getServiceByContractID return an error 0x80040154 when run/debug TWRK40X256QSDLAB MQX3.7

跳至解决方案
2,754 次查看
see
Contributor II

Hi

 

when I was trying to run and debug configuration the TWRK40X256QSDLAB project and the following error appear. I am using Window 7 (32 bit).  can anyone  help? thanks

 

 

org.mozilla.xpcom.XPCOMException: The function "getServiceByContractID" return an error 0x80040154

1 解答
2,270 次查看
mvanlamz
Contributor II

I followed the instructions from this blog post, and now I have no more errors:

 

http://mcuoneclipse.wordpress.com/2012/05/21/fixing-the-morpho-core-exception/

 

Cool!

在原帖中查看解决方案

5 回复数
2,270 次查看
jomar55
Contributor II

I too am having this issue on Windows 7  Professional 64-bit while trying to follow the instructions in FSL_MQX_in_CW_10_x.pdf.

0 项奖励
回复
2,270 次查看
jomar55
Contributor II

I should add that I'm using MQX 3.8 and CW 10.2 on the twrk60 platform.

0 项奖励
回复
2,270 次查看
mvanlamz
Contributor II

I have the same error. I am on Windows 7, CodeWarrior 10.2, MQX 3.8, for the TWR-K60F120M. Before today, I was using OSJTAG over USB, but just now started using the Multilink Universal FX from PE Micro. That's when the errors started.

0 项奖励
回复
2,271 次查看
mvanlamz
Contributor II

I followed the instructions from this blog post, and now I have no more errors:

 

http://mcuoneclipse.wordpress.com/2012/05/21/fixing-the-morpho-core-exception/

 

Cool!

2,270 次查看
jomar55
Contributor II

Great find. Thanks for the update.

0 项奖励
回复