getServiceByContractID return an error 0x80040154 when run/debug TWRK40X256QSDLAB MQX3.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

getServiceByContractID return an error 0x80040154 when run/debug TWRK40X256QSDLAB MQX3.7

ソリューションへジャンプ
3,609件の閲覧回数
see
Contributor II

Hi

 

when I was trying to run and debug configuration the TWRK40X256QSDLAB project and the following error appear. I am using Window 7 (32 bit).  can anyone  help? thanks

 

 

org.mozilla.xpcom.XPCOMException: The function "getServiceByContractID" return an error 0x80040154

1 解決策
3,125件の閲覧回数
mvanlamz
Contributor II

I followed the instructions from this blog post, and now I have no more errors:

 

http://mcuoneclipse.wordpress.com/2012/05/21/fixing-the-morpho-core-exception/

 

Cool!

元の投稿で解決策を見る

5 返答(返信)
3,125件の閲覧回数
jomar55
Contributor II

I too am having this issue on Windows 7  Professional 64-bit while trying to follow the instructions in FSL_MQX_in_CW_10_x.pdf.

0 件の賞賛
返信
3,125件の閲覧回数
jomar55
Contributor II

I should add that I'm using MQX 3.8 and CW 10.2 on the twrk60 platform.

0 件の賞賛
返信
3,125件の閲覧回数
mvanlamz
Contributor II

I have the same error. I am on Windows 7, CodeWarrior 10.2, MQX 3.8, for the TWR-K60F120M. Before today, I was using OSJTAG over USB, but just now started using the Multilink Universal FX from PE Micro. That's when the errors started.

0 件の賞賛
返信
3,126件の閲覧回数
mvanlamz
Contributor II

I followed the instructions from this blog post, and now I have no more errors:

 

http://mcuoneclipse.wordpress.com/2012/05/21/fixing-the-morpho-core-exception/

 

Cool!

3,125件の閲覧回数
jomar55
Contributor II

Great find. Thanks for the update.

0 件の賞賛
返信