example TWR-MEM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

example TWR-MEM

跳至解决方案
8,080 次查看
Microfelix
Contributor IV


hello,


I wanted to know if there are examples of the TWR-MEM with MQX.

 

thanks Maurizio

1 解答
7,341 次查看
DavidS
NXP Employee
NXP Employee

Hello,

The Freescale MQX 3.7\mfs\examples\ramdisk\cw10\mfs_ramdisk_twrk60n512 example can be setup to access MRAM on the TWRMEM card.

I just haven't tried it yet.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
15 回复数
7,341 次查看
DavidS
NXP Employee
NXP Employee

I recently go the TWR-K60N512 kit working with the TWR-MEM Rev B card.

Please reference another thread:

https://community.freescale.com/message/301229

Regards,

David

0 项奖励
回复
7,341 次查看
propellerhead99
Contributor II

Have replaced TWR-MEM board with a new one. Still have same memory read/write problem. Addressability is correct. Simple peek/poke works correctly. Tried several read after write techniques and NOP delays to change timing. Far more errors are counted if I init the memory bits to one rather than zero. Writing with integer boundary rather than byte boundary does not change situation. 

 

I cannot reliably read/write to the TWR-MEM board work with the K60 tower and have submitted a support ticket.

 

0 项奖励
回复
7,341 次查看
propellerhead99
Contributor II

Re: memory test with the K60 tower and TWR-MEM board.

 

When I tested the TWR-MEM MRAM chip using the Freescale test software about 25% of the 512kb bytes were in error.

 

Freescale support reproduced the problem and verified that it is their problem. No answer as to

what will be their next step.

 

 

7,341 次查看
monXii
Contributor III

same problem here..

.. something new???

0 项奖励
回复
7,341 次查看
monXii
Contributor III

removing R14 is not enough!

Remove C2 too!

0 项奖励
回复
7,341 次查看
propellerhead99
Contributor II

I'm newbie to ARM and trying to utilize MRAM. Believe MRAM is interfaced as FlexBus which is addressed at x6000-0000. Looked over example of mfs/example/ramdisk (in Shell_Task) and don't understand how linker moved RAM_DISK_BASE to x6000-0000. It would seem the ram disk was allocated in SRAM. In what units is the ram disk size 0x1800?

Bill

 

0 项奖励
回复
7,341 次查看
DavidS
NXP Employee
NXP Employee

Hi Microfelix,

In general the TWR-MEM card was validated with the TWR-MCF52259.

If you open TWR-MCF52259 projects look for the MRAM target that is using the MRAM on the TWRMEM card.

Hope this helps.

Regards,

David

0 项奖励
回复
7,341 次查看
Microfelix
Contributor IV

 


hello
thanks for the reply.
I have a TWR-K60N512.

I can also find here or should I download the card's documentation that you haveindicated?

0 项奖励
回复
7,342 次查看
DavidS
NXP Employee
NXP Employee

Hello,

The Freescale MQX 3.7\mfs\examples\ramdisk\cw10\mfs_ramdisk_twrk60n512 example can be setup to access MRAM on the TWRMEM card.

I just haven't tried it yet.

Regards,

David

0 项奖励
回复
7,341 次查看
Microfelix
Contributor IV

thanks Maurizio

0 项奖励
回复
7,341 次查看
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

I was making a fast attemp to test the MRAM and found the following the TWR-K60N512.h:

/*
* MRAM cannot be reliably used on TWR_K60N512 due to a hardware conflict unless a hw modification is done:
* disconnecting IrDA receiver e.g. by removing R14 makes MRAM usage possible.
*/
//#define BSP_EXTERNAL_MRAM_RAM_SIZE          ((uint_32)__EXTERNAL_MRAM_RAM_SIZE)

I was able to add the TWR-MEM card to my K60 setup and access the MRAM OK.

Regards,

David

0 项奖励
回复
7,341 次查看
Nana
Contributor II

Maybe in next revision of the  TWR-K60N512 of the board the hardware engineers will put a jumper on that IR led to connect if I want to use that future or if I want to use an external ram memory.

This is only a suggestion i hope will be sent to the devs. 

 

Thank you,

Electronic and Software Engineer

Alexandru Nan

0 项奖励
回复
7,341 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

That modification is already done in TWR-K60 RevD. Is the actual production Tower.

 

Best Regards,

 

Luis

0 项奖励
回复
7,341 次查看
propellerhead99
Contributor II

Using TWR-MEM with K60 tower. Can read/write various MRAM locations with no issue but using a memory

test program in MRAM address space found many bit errors. Have made the IRDA R14 removal. TWR-MEM

jumpered J10 on, J11 off, J16 off.

 

Is my problem jumper configuration, bad board, or ? Does someone have this board/K60 working with no issues?

 

 

 

0 项奖励
回复
7,341 次查看
Microfelix
Contributor IV

thanks david. Begin to test ...

 

maurizio

0 项奖励
回复