ethernet problem on custom board with MQX 3.8.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ethernet problem on custom board with MQX 3.8.1

Jump to solution
1,295 Views
khoanguyen
Contributor I

Hi,

My project includes creating a custom board with ethernet and ADC functionality, with MQX 3.8.1, CW 10.2, and the k60 tower development.

So far the custom board has been successful with all but the ethernet transceiver. We've chosen the same ethernet transceiver on the K60 dev kit, but we're now at a standstill on what could be going wrong since we followed the schematics and double checked them.

The custom board is able to have code flashed onto and run successfully on MQX demos, except for any ethernet required demos. When an ethernet cord is plugged into the custom board and a computer, neither of the lights are on so there is no connection, but I'm assuming this is a hardware problem.

I was wondering if this could be a hardware problem or software problem? Do the BSP/PSP config files have to be reformatted to the custom board, even though it works with the MQX ADC demo using the kinetis bsp/psp files?

Thanks,

Khoa Nguyen


Tags (3)
0 Kudos
Reply
1 Solution
887 Views
macl
Senior Contributor I

Hi,

Is the ethernet phy bootstrap resistor configuration set the same?  Are you using RMII or MII mode?  On the TWR-K60 + TWR-SER modules, for RMII, the 50MHz clock on the TWR-SER is fed to both the K60 MCU and ethernet phy clock input to keep them in sync.  MII clocking is a bit different.

If you use the same phy and the same mode, then I don't think any changes would be necessary in the BSP.  Just make sure the phy is working.

Best of luck,

Mac

View solution in original post

0 Kudos
Reply
1 Reply
888 Views
macl
Senior Contributor I

Hi,

Is the ethernet phy bootstrap resistor configuration set the same?  Are you using RMII or MII mode?  On the TWR-K60 + TWR-SER modules, for RMII, the 50MHz clock on the TWR-SER is fed to both the K60 MCU and ethernet phy clock input to keep them in sync.  MII clocking is a bit different.

If you use the same phy and the same mode, then I don't think any changes would be necessary in the BSP.  Just make sure the phy is working.

Best of luck,

Mac

0 Kudos
Reply