egui image loading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

egui image loading

跳至解决方案
1,267 次查看
Toe
Contributor IV

Is there a simple way to load images from another type of flash device without having to copy them to local flash?  If I had some images on an sd card, usb, or some other serial flash, how can I load these as I need them without declaring them as part of the screen before hand?

0 项奖励
回复
1 解答
1,101 次查看
Gargy
NXP Employee
NXP Employee

Hi,

the new version (not released yet) support external bitmap *.BMP file.

You can look at it in this thread:

https://community.freescale.com/message/100414#100414

 

Petr

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,102 次查看
Gargy
NXP Employee
NXP Employee

Hi,

the new version (not released yet) support external bitmap *.BMP file.

You can look at it in this thread:

https://community.freescale.com/message/100414#100414

 

Petr

0 项奖励
回复