egui image loading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,689件の閲覧回数
Toe
Contributor IV

Is there a simple way to load images from another type of flash device without having to copy them to local flash?  If I had some images on an sd card, usb, or some other serial flash, how can I load these as I need them without declaring them as part of the screen before hand?

0 件の賞賛
返信
1 解決策
1,523件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hi,

the new version (not released yet) support external bitmap *.BMP file.

You can look at it in this thread:

https://community.freescale.com/message/100414#100414

 

Petr

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,524件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hi,

the new version (not released yet) support external bitmap *.BMP file.

You can look at it in this thread:

https://community.freescale.com/message/100414#100414

 

Petr

0 件の賞賛
返信