egui image loading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

egui image loading

Jump to solution
1,634 Views
Toe
Contributor IV

Is there a simple way to load images from another type of flash device without having to copy them to local flash?  If I had some images on an sd card, usb, or some other serial flash, how can I load these as I need them without declaring them as part of the screen before hand?

0 Kudos
Reply
1 Solution
1,468 Views
Gargy
NXP Employee
NXP Employee

Hi,

the new version (not released yet) support external bitmap *.BMP file.

You can look at it in this thread:

https://community.freescale.com/message/100414#100414

 

Petr

View solution in original post

0 Kudos
Reply
1 Reply
1,469 Views
Gargy
NXP Employee
NXP Employee

Hi,

the new version (not released yet) support external bitmap *.BMP file.

You can look at it in this thread:

https://community.freescale.com/message/100414#100414

 

Petr

0 Kudos
Reply