eGUI alternate language string table prefix won't change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eGUI alternate language string table prefix won't change

6,748件の閲覧回数
GeneGoff
Contributor III

The eGUI demo for the TWR-K70 has a language selection example which uses the D4D_STRINGTABLE_PREFIX character '@' to intercept the string and divert it to a different language string table.  However, I want to use the @ character as the displayed text title on a button, such as in a QWERTY keyboard application.  Since the @ character in a string has a special meaning, it won't display as the button text title.  It seemed the easiest workaround would be to simply use a different ASCII character such as $.  So I replaced every occurance of the @ character with the $ character concerning the D4D_STRINGTABLE_PREFIX and in the string table itself.  It did not work, all the strings displayed the literal "$01", "$02" etc. 

Anyone know how to use a different reserved character for the D4D_STRINGTABLE_PREFIX?

タグ(1)
0 件の賞賛
返信
12 返答(返信)

6,112件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Gene,

Please change the macro D4D_STRINGTABLE_PREFIX in the files "d4d_user_cfg_app.h" and "strings.h". Do not forget to rebuild the D4D library when you change something.

1. Change the macro D4D_STRINGTABLE_PREFIX in the files "d4d_user_cfg_app.h" and "strings.h".

#define D4D_STRINGTABLE_PREFIX '$'

2. Replace the "@" character by "$" in the file "strings.h".

// String names

#define D4D_STR_OPEN                          D4D_DEFSTR("$00")

#define D4D_STR_OPENFILE                      D4D_DEFSTR("$01")

#define D4D_STR_CLOSE                         D4D_DEFSTR("$02")

#define D4D_STR_CANCEL                        D4D_DEFSTR("$03")

#define D4D_STR_OK                            D4D_DEFSTR("$04")

#define D4D_STR_SYSTEM                        D4D_DEFSTR("$05")

#define D4D_STR_DIRECTORIES                   D4D_DEFSTR("$06")

#define D4D_STR_FILES                         D4D_DEFSTR("$07")

#define D4D_STR_DISK                          D4D_DEFSTR("$08")

#define D4D_STR_LANG                          D4D_DEFSTR("$09")

#define D4D_STR_LANGEN                        D4D_DEFSTR("$10")

#define D4D_STR_LANGCZ                        D4D_DEFSTR("$11")

#define D4D_STR_LANGCHI                       D4D_DEFSTR("$12")

#define D4D_STR_LANGRES1                      D4D_DEFSTR("$13")

#define D4D_STR_LANGRES2                      D4D_DEFSTR("$14")

#define D4D_STR_LANGRES3                      D4D_DEFSTR("$15")

#define D4D_STR_LANGRES4                      D4D_DEFSTR("$16")

#define D4D_STR_SETTINGS                      D4D_DEFSTR("$17")

#define D4D_STR_SCHEME                        D4D_DEFSTR("$18")

#define D4D_STR_SCHEME_GREY                   D4D_DEFSTR("$19")

#define D4D_STR_SCHEME_GREEN                  D4D_DEFSTR("$20")

#define D4D_STR_SCHEME_BLUE                   D4D_DEFSTR("$21")

#define D4D_STR_SCHEME_RED                    D4D_DEFSTR("$22")

#define D4D_STR_FONTS                         D4D_DEFSTR("$23")

#define D4D_STR_FONTS_COURIER                 D4D_DEFSTR("$24")

#define D4D_STR_FONTS_ARIAL                   D4D_DEFSTR("$25")

#define D4D_STR_SCRSVR                        D4D_DEFSTR("$26")

#define D4D_STR_ENABLE                        D4D_DEFSTR("$27")

#define D4D_STR_DUMMY_LABEL                   D4D_DEFSTR("$28")

#define D4D_STR_COULD_NOT_SHOW                D4D_DEFSTR("$29")

#define D4D_STR_IMAGE_INFO                    D4D_DEFSTR("$30")

#define D4D_STR_TYPE                          D4D_DEFSTR("$31")

#define D4D_STR_WIDTH                         D4D_DEFSTR("$32")

#define D4D_STR_HEIGHT                        D4D_DEFSTR("$33")

#define D4D_STR_SIZE                          D4D_DEFSTR("$34")

#define D4D_STR_TEXT_INFO                     D4D_DEFSTR("$35")

#define D4D_STR_ASCII                         D4D_DEFSTR("$36")

#define D4D_STR_UNICODE                       D4D_DEFSTR("$37")

#define D4D_STR_INFO                          D4D_DEFSTR("$38")

#define D4D_STR_UNKNOWN                       D4D_DEFSTR("$39")

3. You can use the character "@" in the strings in the file "strings.c". For example:

D4D_DEFSTR("@Open"),               // D4D_STR_OPEN

4. Rebuild all.

pastedImage_7.png

5. Enjoy the "@" character Smiley Happy.

pastedImage_9.jpg

Best regards,

Earl Orlando.

/* If this post answers your question please click the Correct Answer button */

6,112件の閲覧回数
GeneGoff
Contributor III

I fixed my problem - I changed project and library names but did not change the Linker's Additional Libraries paths, so it was using an old library build.   

Again, there was no Correct Answer button shown, only "Like . Helpful Yes|No . Reply . Actions", so the best thing available was Helpful Yes.

6,112件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Gene,

Could you please sign in and take an screenshot of your post where the Correct Answer button does not show? I need to report this issue.

Regards,

Earl.

0 件の賞賛
返信

6,112件の閲覧回数
GeneGoff
Contributor III

Earl, here is a screen shot.  I don't see any "Correct Answer" button.

pastedImage_0.png

6,112件の閲覧回数
admin
Specialist II

Hi [email protected]​, a question related to non being able to see the Correct Answer button:

Is this the only thread you are not able to see the "Correct Answer" button? Are you able to see that option in other threads you've created?

Have you tried from a different browser?

Can you please confirm you don't have any browser plugins such as ad-blocker or similar which can prevent to show part of web sites?

Thanks!

Denisse

0 件の賞賛
返信

6,112件の閲覧回数
GeneGoff
Contributor III

1) No, I have had several threads where I see no "Correct Answer"

button. A screen shor is copied below where I just post a new question

and Earl replied and there is no Correct Answer button.

2) I have tried Firefox and Chrome and saw the same result.

3) I checked and do not have any ad-blocking plug-ins.

Thank you,

Gene

Screen shot showing no "Correct Answer" button:

0 件の賞賛
返信

6,112件の閲覧回数
admin
Specialist II

Thanks for you reply-

0 件の賞賛
返信

6,112件の閲覧回数
admin
Specialist II

GeneGoff I found another another community account with the same name: [email protected]

Is it yours? If so, can we delete it?

This button missing can only happen if Jive doesn't recognize you as the author (which could be the case), or an error during the page loading.

0 件の賞賛
返信

6,112件の閲覧回数
GeneGoff
Contributor III

I do have a work and home Freescale account, each with a different email and different Codewarrior license because of separate business activity. The only thing which is the same is the "nickname" Gene Goff which I would not think would cause a "Correct Answer" button to not be displayed in the web page.

-


Karla Denisse Mendoza Almanzar <[email protected]> wrote:

Karla Denisse Mendoza Almanzar mentioned you in in Freescale Community.

Participate in the conversation by replying to this email, or to view Karla Denisse Mendoza Almanzar's reference to you, visit: https://community.freescale.com/message/526548?et=notification.mention#526548

This email was sent by Freescale Community because you are a registered user.

You may unsubscribe instantly at https://community.freescale.com/unsubscribe.jspa?email=ggoff%40rochester.rr.com&token=966c9ae66fd8d6..., or adjust email frequency in your email preferences (https://community.freescale.com/user-preferences!input.jspa).

0 件の賞賛
返信

6,112件の閲覧回数
admin
Specialist II

Thanks for your reply.
I see both community profiles have the exact same name and last name. Can I give it a try changing one of them so that they don't match?

Any suggested name or last name to make them differ?

Denisse

0 件の賞賛
返信

6,112件の閲覧回数
EarlOrlando
Senior Contributor II

In this post occurs the same problem.

Regards,

Earl.

0 件の賞賛
返信

6,113件の閲覧回数
EarlOrlando
Senior Contributor II

Thank you!

Have a great day Gene,

Earl.

0 件の賞賛
返信