connecting to http server over internet (Public IP address of ISP)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

connecting to http server over internet (Public IP address of ISP)

1,651件の閲覧回数
vallinaths
Contributor II

Please can anybody put the limelight how can we access the private LAN on internet ,

webserver implemented on the card . and webpages are mounted on the SD card

Setup:

a)Card having K60 with ethernet port on private LAN with IP:192.168.10.5 Port:80 acess the webpages the link used http:192.168.10.5:80/SDcard/web_pages/index.html

b)Wifi router is available on which Internet connection is available(ISP) connectivity to outer world.The card is connected to the router .

c) Now in the router added the virtual route to forward the public IP adress port 80 to private LAN .

In private LAN we are able to reach the card http:192.168.10.5:80/SDcard/web_pages/index.html.

But how to get access the card using the pubilc network that is threw internet . Please let me know anyother configuration to be made on the card to reach to outer world.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,351件の閲覧回数
vallinaths
Contributor II

Hi soledad ,

  Thanks for the reply , I went threw the application notes , it mentions about discovery .

Is there a way  we reach the private LAN MQX device on the public Network , I have enabled port forwarding option in router but still not able to achieve the desire result

Can you put some lime light on it

regards

vallinath

0 件の賞賛
返信

1,351件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello vallinath:

Please check the below application notes:

http://cache.freescale.com/files/32bit/doc/app_note/AN4644.pdf

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4417.pdf?fasp=1&WT_TYPE=Application...

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4810.pdf?fasp=1&WT_TYPE=Application...


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信