connecting to http server over internet (Public IP address of ISP)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

connecting to http server over internet (Public IP address of ISP)

1,638 Views
vallinaths
Contributor II

Please can anybody put the limelight how can we access the private LAN on internet ,

webserver implemented on the card . and webpages are mounted on the SD card

Setup:

a)Card having K60 with ethernet port on private LAN with IP:192.168.10.5 Port:80 acess the webpages the link used http:192.168.10.5:80/SDcard/web_pages/index.html

b)Wifi router is available on which Internet connection is available(ISP) connectivity to outer world.The card is connected to the router .

c) Now in the router added the virtual route to forward the public IP adress port 80 to private LAN .

In private LAN we are able to reach the card http:192.168.10.5:80/SDcard/web_pages/index.html.

But how to get access the card using the pubilc network that is threw internet . Please let me know anyother configuration to be made on the card to reach to outer world.

Labels (1)
0 Kudos
Reply
2 Replies

1,338 Views
vallinaths
Contributor II

Hi soledad ,

  Thanks for the reply , I went threw the application notes , it mentions about discovery .

Is there a way  we reach the private LAN MQX device on the public Network , I have enabled port forwarding option in router but still not able to achieve the desire result

Can you put some lime light on it

regards

vallinath

0 Kudos
Reply

1,338 Views
soledad
NXP Employee
NXP Employee

Hello vallinath:

Please check the below application notes:

http://cache.freescale.com/files/32bit/doc/app_note/AN4644.pdf

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4417.pdf?fasp=1&WT_TYPE=Application...

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4810.pdf?fasp=1&WT_TYPE=Application...


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply