ZeroG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,995 Views
TonyP_
Contributor I

Hi,

 

I know an earlier version of the MQX works with ZeroG's 2101M. Our design uses that part. Now you have MQX 3.6. Does v. 3.6 still work with the ZeroG module? In other words, should we update to 3.6 or stay with the earlier MQX version?

 

Thanks,

Tony

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,459 Views
PetrL
NXP Employee
NXP Employee

Hi,

 

there shouldn't be problem in using ZeroG driver in MQX 3.6 . The MQX enet driver API is still the same as it was in the time ZeroG was released.

 

You can check change log of the MQX 3.6 (in the Release Notes) and figure out if the features/bugfixes are relevant for your platform and your application. If you decide to switch to 3.6 then it is better to wait 2-3 weeks. In that time should be MQX 3.6.1 released - this version brings several bug fixes.

 

Regards,

PetrL

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
1,460 Views
PetrL
NXP Employee
NXP Employee

Hi,

 

there shouldn't be problem in using ZeroG driver in MQX 3.6 . The MQX enet driver API is still the same as it was in the time ZeroG was released.

 

You can check change log of the MQX 3.6 (in the Release Notes) and figure out if the features/bugfixes are relevant for your platform and your application. If you decide to switch to 3.6 then it is better to wait 2-3 weeks. In that time should be MQX 3.6.1 released - this version brings several bug fixes.

 

Regards,

PetrL

 

 

 

0 Kudos
Reply