ZeroG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,019件の閲覧回数
TonyP_
Contributor I

Hi,

 

I know an earlier version of the MQX works with ZeroG's 2101M. Our design uses that part. Now you have MQX 3.6. Does v. 3.6 still work with the ZeroG module? In other words, should we update to 3.6 or stay with the earlier MQX version?

 

Thanks,

Tony

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,483件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

 

there shouldn't be problem in using ZeroG driver in MQX 3.6 . The MQX enet driver API is still the same as it was in the time ZeroG was released.

 

You can check change log of the MQX 3.6 (in the Release Notes) and figure out if the features/bugfixes are relevant for your platform and your application. If you decide to switch to 3.6 then it is better to wait 2-3 weeks. In that time should be MQX 3.6.1 released - this version brings several bug fixes.

 

Regards,

PetrL

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,484件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

 

there shouldn't be problem in using ZeroG driver in MQX 3.6 . The MQX enet driver API is still the same as it was in the time ZeroG was released.

 

You can check change log of the MQX 3.6 (in the Release Notes) and figure out if the features/bugfixes are relevant for your platform and your application. If you decide to switch to 3.6 then it is better to wait 2-3 weeks. In that time should be MQX 3.6.1 released - this version brings several bug fixes.

 

Regards,

PetrL

 

 

 

0 件の賞賛
返信