What's the difference between driver NAME and NAME_LDD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the difference between driver NAME and NAME_LDD?

1,122 Views
jvasil
Contributor III

Some components both a high-level driver (eg ExtInt) and a low-level driver (eg ExtInt_LDD)--is there something that describes the differences and when each should be used?  The components that have both that I've looked at seem to have similar functionality and I didn't find anything in the MQX Lite User Guide or Reference Manual that describes this.

0 Kudos
Reply
1 Reply

985 Views
adriancano
NXP Employee
NXP Employee

Hi,

In the Processor Expert information you can find that topic.

Please refer to this thread which has a similar question:

difference between ExtInt and ExtInt_LDD

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply