What's the difference between driver NAME and NAME_LDD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between driver NAME and NAME_LDD?

1,118件の閲覧回数
jvasil
Contributor III

Some components both a high-level driver (eg ExtInt) and a low-level driver (eg ExtInt_LDD)--is there something that describes the differences and when each should be used?  The components that have both that I've looked at seem to have similar functionality and I didn't find anything in the MQX Lite User Guide or Reference Manual that describes this.

0 件の賞賛
返信
1 返信

981件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

In the Processor Expert information you can find that topic.

Please refer to this thread which has a similar question:

difference between ExtInt and ExtInt_LDD

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信