Using the Mini-Flex-Bus for external RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using the Mini-Flex-Bus for external RAM

跳至解决方案
3,583 次查看
Stefan_75
Contributor II

Hi,

 

I want to use the Mini-Flex-Bus for accessing external RAM (MCF52259). There is no driver availible for this. Therefore I tried to configure the needed pins in the bsp part of the MQX system. But even there I can´t access the pins that I need for.

 

Is ther any way to solve this easily?

 

Thanks for any hint.

 

Stefan

0 项奖励
回复
1 解答
2,714 次查看
JaimeR
Contributor III

Check this thread. That should get you started.

 

 External RAM

 

Message Edited by Jaime R on 2009-10-26 03:16 PM

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,714 次查看
kleckerspur
Contributor III

link seem to be brocken !

0 项奖励
回复
2,714 次查看
kleckerspur
Contributor III

link seems to be brocken

External RAM links to ....

Welcome | Freescale Community

0 项奖励
回复
2,715 次查看
JaimeR
Contributor III

Check this thread. That should get you started.

 

 External RAM

 

Message Edited by Jaime R on 2009-10-26 03:16 PM
0 项奖励
回复
2,714 次查看
Stefan_75
Contributor II

Thanks. That´s it.

 

STefan

0 项奖励
回复