Using the Mini-Flex-Bus for external RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the Mini-Flex-Bus for external RAM

ソリューションへジャンプ
3,686件の閲覧回数
Stefan_75
Contributor II

Hi,

 

I want to use the Mini-Flex-Bus for accessing external RAM (MCF52259). There is no driver availible for this. Therefore I tried to configure the needed pins in the bsp part of the MQX system. But even there I can´t access the pins that I need for.

 

Is ther any way to solve this easily?

 

Thanks for any hint.

 

Stefan

0 件の賞賛
返信
1 解決策
2,817件の閲覧回数
JaimeR
Contributor III

Check this thread. That should get you started.

 

 External RAM

 

Message Edited by Jaime R on 2009-10-26 03:16 PM

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,817件の閲覧回数
kleckerspur
Contributor III

link seem to be brocken !

0 件の賞賛
返信
2,817件の閲覧回数
kleckerspur
Contributor III

link seems to be brocken

External RAM links to ....

Welcome | Freescale Community

0 件の賞賛
返信
2,818件の閲覧回数
JaimeR
Contributor III

Check this thread. That should get you started.

 

 External RAM

 

Message Edited by Jaime R on 2009-10-26 03:16 PM
0 件の賞賛
返信
2,817件の閲覧回数
Stefan_75
Contributor II

Thanks. That´s it.

 

STefan

0 件の賞賛
返信