Using KDS_3.0.0 KSDK_1.2.0 Can't get MQX Task List or MQX Stack Usage to show.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using KDS_3.0.0 KSDK_1.2.0 Can't get MQX Task List or MQX Stack Usage to show.

934件の閲覧回数
georgejoseph
Contributor III

I'm working on a board with a K64 processor, KDS_3.0.0 KSDK_1.2.0 tools, MQX.  At one point in the project the Task List and Stack Usage became unavailable. I have gone back previous versions of the project where I know it was working, but no longer works, so it's not related to  project settings or stack size as I have seen in other posts. The error log shows:

pastedImage_1.png

and the MQX Task List tab shows:

pastedImage_2.png

Task aware debugger is installed:

pastedImage_3.png

Any ideas?

0 件の賞賛
返信
2 返答(返信)

799件の閲覧回数
georgejoseph
Contributor III

Update: 

I removed the MQX Task List tab from the window

pastedImage_1.png

and re-added it back and the task list and it was restored.

pastedImage_2.png

Selected Other then selected MQX Task List from the MQX folder.

pastedImage_3.png

0 件の賞賛
返信

799件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi George Joseph

I tried the MQX task list with KDS 3.2, and it can work.

It seems that MQX RTOS Task Aware Debugger for GDB is missing in you KDS installation.

pastedImage_1.png

Regards

Daniel

0 件の賞賛
返信